IMMI Safety Precautions
| Description |
This section contains safety precautions specific to installing the IMMI.
Unauthorized modification of the IMMI module can result in personnel injury or equipment damage.
The absence of protection at the mold area to prevent access, or to detect presence in the mold area, can result in personnel injury or equipment damage.
The Mould Area Free (MAF) signals are not intended for safeguarding.
Failure to coordinate the movement between the robot arm and the IMM can result in personnel injury or equipment damage.
|
|
Failure to connect the ground (GND) wire during installation can result in equipment damage.
Disconnecting the ribbon cable when the control box is powered on can result in equipment damage.
|
| Emergency Stop |
The robot and the IMM send Emergency Stop safety signals to each other through the IMMI. When a UR emergency stop is triggered, both the robot stops and the IMMI signals a stop to the IMM. Ensure all Emergency Stops halt the entire application before operating the application. |
| Safeguard Stop
|
When the UR robot Safeguard Stop is triggered by the IMM, the robot stops. Reaching into the IMM workspace can lead to serious personnel injury.
|