General Safety Precautions

Description

This section contains general safety precautions, read it before installing the IMMI.

For more information on safety, refer to the Safety section in the robot User Manual.

Installing or maintaining equipment connected to a power source can lead to electric shock.

  • Disconnect the equipment from the power source before installation or maintenance.

Incorrect connection of the power source or ground wires can result in personnel injury or equipment damage.

Damage caused by invalid power source connection is not covered by warranty. Before starting the operation:

  • Ensure the power source wiring is correct.
  • Ensure the grounding is correct.

Failure to verify and validate safeguarding and functionality can result in death or serious injury.

  • Ensure all risk reduction works as intended and achieves the needed risk reduction.

Failure to perform a risk assessment before installation and operation can result in personnel injury or equipment damage.

  • Perform a risk assessment before installation and operation.

  • Read the UR User Manual and UR Service Manual.

This product includes the Universal Robots e-Series robot. General safety considerations that are valid for the Universal Robots e-Series robot are also valid for this product.

Failure to use the robot as described in the User Manual can lead to personnel injury.

  • For more information on safety, refer to the Safety section in the Universal Robots e-Series robot User Manual.