Teach Pendant (TP7)

Description

The TP7 is the standard Teach Pendant for the g-Series robot system. It provides a user interface for operating, programming, and monitoring the robot during installation, setup, and manual operation.

TP7 is designed as a handheld device that can be carried by a single person and used directly at the robot cell. When not in use, it can be mounted on a wall or on the Control Box using a dedicated mounting bracket.

 

Software

The TP7 is a third-party product, manufactured for Universal Robots. Its software, including the operating system and the application that displays PolyScope X, is developed and maintained by the supplier to Universal Robots' specifications. PolyScope X itself is developed by Universal Robots. Software composition is known to Universal Robots and documented in the software bill of materials (SBOM). By default, the TP7 communicates only with the Control Box. In a future version of PolyScope X, an administrator will be able to turn on network access for the TP7.

 

The USB port on the TP7 can only be used to connect keyboard or mouse.
Always use the USB port on the Control box to upgrade the software.

CB7 Core does not support the Universal Robots 3PE Teach pendant.

 

 

The unit includes a touchscreen interface and integrated safety controls, enabling the operator to interact with the robot and perform manual movements under controlled conditions. In configurations equipped with a 3-Position Enabling device, robot motion during manual operation requires continuous operator engagement.

 

TP7 has two user-configurable buttons, each of which can be assigned a Smart Skill in PolyScope X. When a button is pressed, it executes the selected Smart Skill.

 

1 Power button 4 TP7 Smart buttons
2 Emergency stop button 5 3PE buttons (ambidextrous)
3 USB port (comes with a removable dust cover)    
TP7 controls