Gripper Module
| Description |
Grippers are devices that enable robots to pick up and hold objects. When combined with the robot arm, grippers enable you to automate processes, such as inspection, assembly, pick and place, and machine tending. Similar to the human hand, grippers are positioned at the end of the arm, functioning as end effector, and their abilities allow you to combine the strength of an arm with the dexterity of a hand. When you create a gripper module, you optimize ease, readability, and flexibility in using its appropriate command nodes.
|
|
To create Gripper module |
|
|
|
|