Header

Description

The header contains three functioning menus and feature:

  • Hamburger menu

  • System manager or Program name menu

  • Safety checksum

 

To open the Hamburger menu

 

 

To open Program name

When you tap the Program name menu, the System Manager screen appears, which enables you to do several things:

  • View a list of all installed programs

  • See the loaded program, marked Active

  • Create new programs

  • Open a created program

  • Search programs

  • Import and export a program

  • Load a program

 
  • Install URCaps

  • Ensure the software license

  • Add a script file

  • Write a program description

  • See program details

  • View script

 

To open Safety checksum

Tap the Safety checksum icon on the right side of the header to open the robot’s Safety Overview. The items in the Safety Overview panel correspond to the safety settings you configured in the Application tab. Use the scroll bar to review your complete safety configuration.

This icon shows the default Safety checksum for a newly created program in a new application.