Freedrive Input
| Description |
Freedrive input is recommended to be used with 3PE TP and/or 3 Position Enabling Device input. When Freedrive INPUT is
|
| Freedrive Enabled Input |
On UR8 Long robots, the Freedrive Enabled Input and 3-Position Switch safety functions can be assigned to the Tool Inputs on the application Safety screen.
This functionality is currently only available on the UR8 Long robots. On all other robot types, the new Tool Inputs section is not shown on the Safety I/O screen.
|
|
|
When the Tool inputs are assigned a Safety Function, it is not possible to rename a Tool input or assign a Tool input an action on the Communication Tool IO screen.
|