Settings
| Description |
The settings in PolyScope X can be accessed via the hamburger menu in the main navigation. You can access the following sections:
|
|
General Settings |
In the general settings, you can change the preferred language, units of measurements, etc. You also update the software from the general settings. |
|
Password Settings |
In the password settings, you can find the default passwords, and how to change them to the preferred and secure passwords. |
| Connection Settings |
In the connection settings, you can set network settings such as IP address, DNS server, etc. Settings related to UR Connect is also found here. |
|
Security Settings |
The security settings related to SSH, admin password permissions and enabling/disabling of various services in the software.
|