Robot Connections: Robot Cable

Description

This subsection describes the connection for a robot arm configured with a fixed 6 meter Robot Cable.

 

To connect the arm and Control box

You can turn the connector to the right to make it easier to lock after the cable is plugged in.

  • Establish the robot connection by connecting the robot arm to the Control Box with the Robot Cable.

  • Plug and lock the cable from the robot into the connector at the bottom of the Control Box shown below.

  • Twist the connector twice to ensure it is properly locked before turning on the robot arm.

 

 

Improper robot connection can result in loss of power to the robot arm.

  • Do not disconnect the Robot Cable when the robot arm is turned on.

  • Do not modify the original Robot Cable.