Electrical Warnings and Cautions
| Warnings |
Observe the following warnings for all the interface groups, including when you design and install an application.
|
|
Failure to follow any of the below can result in serious injury or death, as the safety functions could be overridden.
|
|
Failure to follow any of the below can result in serious injury or death due to electrical hazards.
|
|
Disturbing signals with levels higher than those defined in the specific IEC standards can cause unexpected behaviors from the robot. Be aware of the following:
|
|
Negative connections are referred to as Ground (GND) and are connected to the casing of the robot and the Control Box. All mentioned GND connections are only for powering and signalling. For PE (Protective Earth) use the M6-size screw connections marked with earth symbols inside the Control Box. The grounding conductor shall have at least the current rating of the highest current in the system. |
|
Some I/Os inside the Control Box can be configured for either normal or safety-related I/O. Read and understand the complete Electrical Interface chapter. |