Validity and Responsibility

Description

The information in this manual does not cover designing, installing, integrating and operating a robot application, nor does it cover all peripheral equipment that can influence the safety of the robot application.

 

The robot application must be designed and installed in accordance with the safety requirements set forth in the relevant standards and regulations of the country where the robot is installed.

 

The person/s integrating the AI Accelerator are responsible for ensuring the applicable regulations in the country concerned are observed and that any risks in the robot application are adequately reduced. This includes, but is not limited to:

  • Performing a risk assessment for the complete robot system

  • Interfacing other machines and additional safeguarding if required by the risk assessment

  • Setting the correct safety settings in the software

  • Ensuring safety measures are not modified

  • Validating the robot application is designed, and installed and integrated

  • Specifying instructions for use

  • Marking the robot installation with relevant signs and contact information of the integrator

  • Retaining all documentation; including the application risk assessment, this manual, robot manual and additional relevant documentation.