Intended Use
| Description |
The AI Accelerator is intended to create robot applications using Pereception, AI and PolyScope X integraton solution.
Possible applications of AI Accelerator are limited by combination of the technical specifications of it's components. Consult technical specification of individual components to determine their suitability for a purpose.
For details about the conditions under which the robot should operate, see Declarations and Certificates and the technical specifications in the robot User Manual.
All UR robots are equipped with safety functions, which are purposely designed to enable collaborative applications, where the robot application operates together with a human. The safety function settings must be set to the appropriate values as determined by the robot application risk assessment.
Collaborative applications, without guards or protective devices, are only intended for non-hazardous applications, where the complete application, including tool/end effector, work piece, obstacles and other machines, is low risk according to the risk assessment of the specific application. The AI Accelerator shall not be used with CB3 robots or PolyScope versions prior to 10.7.1.
|
|
Using UR robots or UR products outside of the intended uses can result in injuries, death and/or property damage. Do not use the UR robot or products for any of the below unintended uses and applications:
UNIVERSAL ROBOTS EXPRESSLY DISCLAIMS ANY EXPRESS OR IMPLIED WARRANTY OF FITNESS FOR ANY PARTICULAR USE. |
Failure to use the AI Accelerator in accordance with the intended use can result in unsafe situations.
|