Connectivity

Description

This section describes the connection of the components of the AI Accelerator

Do not use any cables if they are damaged or show signs of wear.

 

  1. Robot Arm
    Connected to Control Box with proprietary cable.

  2. Control Box
    Connected to the mains power (not shown).

  3. Teach Pendant
    Connected to the Control Box with proprietary cable.

  4. Compute module
    Connected to Control Box via Ethernet connection. Initial setup requires monitor, keyboard and mouse (not included).

  5. Camera
    Connected to Compute module with supplied camera cable.