Assembling the AI Accelerator

Description

Complete assembly of AI Accelerator requires the following steps:

  1. Mounting the robot

  2. Attaching camera mount and optionally an end effector (SeeAttaching the Camera Mount )

  3. Affixing camera cable (See Camera cable)

  4. Connecting Ethernet cables

  5. Connecting power cables

 

Mounting the robot

For mechanical and electrical installation instructions of the robot arm and the Control Box, refer to the robot User Manual.