com.ur.urcap.api.ui.component
public interface InputCheckBox extends HTMLComponent
Represents an input checkbox UI component
| Modifier and Type | Method and Description |
|---|---|
String |
getText() |
boolean |
isSelected() |
void |
setSelected(boolean selectedState) |
void |
setText(String text) |
isEnabled, isVisible, setEnabled, setVisiblevoid setText(String text)
text - set the text associated with the input check boxString getText()
boolean isSelected()
void setSelected(boolean selectedState)
selectedState - make checkbox checked if true and unchecked otherwise.Copyright © 2017. All rights reserved.