com.ur.urcap.api.ui.component
public interface InputButton extends HTMLComponent
Represents an input button UI component
| Modifier and Type | Method and Description |
|---|---|
Image |
getImage() |
String |
getText() |
void |
setImage(Image icon) |
void |
setText(String text) |
isEnabled, isVisible, setEnabled, setVisiblevoid setText(String text)
text - set the text inside the button.String getText()
void setImage(Image icon)
icon - set an icon inside the buttonImage getImage()
null if no icon is set.Copyright © 2017. All rights reserved.