AI Pipe Welding System for Universal Robots

AI Pipe Welding System for Universal Robots
AI Pipe Welding System for Universal Robots

ARC Specialties selects Universal Robots as ‘Golden Arm’ in New Artificial Intelligence Pipe Welding System Launching at OTC 2019

ARC Specialties has solved the challenge of creating repeatable full penetration pipe welds by combining AI, advanced sensors, and the UR5 collaborative robot from Universal Robots. The unique Artificial Intelligence Pipe Welding System debuts at the Offshore Technology Conference in Houston, May 6-9.

The toughest welds to make are full penetration, single sided, V butt, pipe welds. Historically, ARC Specialties, a Houston-based developer of welding solutions, declined these jobs because joint fit-up was never repeatable. “Only human welders with a ‘golden arm’ able to compensate for variation in root openings, weld center lines, and groove volumes could handle this challenge,” says Dan Allford, President of ARC Specialties. “With the industry facing labor shortages, we decided to develop an intelligent machine with complete knowledge of pipe welding, with full motion and welding control.”

Video

The Artificial Intelligence Pipe Welding System (AIPW) incorporates the 6-axis UR5 collaborative robot arm from Universal Robots to carry out the challenging welds. “The UR5 now becomes our ‘golden arm’,” says Allford. “The UR5 is small enough to be portable yet still allows full freedom of motion for both the laser scanner and welding torch. Being collaborative the robot is able to safely work in close proximity to humans.” The AIPW officially launches at ARC Specialties’ booth 705 at the Offshore Technology Conference held in Houston, TX, May 6-9.

Stuart Shepherd, Regional Sales Director of Universal Robots’ Americas division, is delighted to see the UR5 power ARC’s AIPW system. “This implementation underscores our collaborative robots’ ability to handle heavy-duty processing tasks that demand both high precision and real-time adaptability,” he says. “We’re excited to share this solution with the oil and gas industry.”

The AIPW pre-scans the root opening (gap) using a 2D laser, then uses the data to generate the robot path and welding parameters. Gap variations are compensated for with changes in oscillation, torch position, travel speed and welding conditions. The UR5 positions the torch over a tack weld to start the arc to insure 100% root weld acceptance. Fill and cap pass programs are optimized to fill the groove using user selectable weave or stringer bead welding techniques. The AIPW uses the Miller Auto Continuum welding power supply to weld the root with Regulated Metal Deposition (RMD), then switches to pulsed spray for the fill and cap passes. This combination of Gas Metal Arc Welding techniques maximizes welding productivity while producing X-Ray quality, full penetration pipe welds.

The AIPW follows two other successful welding solutions featuring Universal Robots developed by ARC Specialties; the MIG welding SnapWeld and the plasma cutting SnapCut. SnapWeld just became the first product ever to win New Equipment Digest’s Innovation Award two years in a row.

Universal Robots

Universal Robots

We believe that collaborative robotic technology can be used to benefit all aspects of task-based businesses – no matter what their size.

We believe that the latest collaborative robot technology should be available to all businesses. The nominal investment cost is quickly recovered as our robotic arms have an average payback period of just six months.

Local Office
  • Universal Robots USA, Inc
  • 27175 Haggerty Road, Suite 160
  • 48377 Novi, MI
Contact us: +1 844-462-6268
UR Hotline: + 1-844-GO-COBOT