How to Get a 6-Axis Robot for the Price of a 3-Axis

For small and mid-sized manufacturers who are exploring robotics, the decision on 3-axis or 6-axis movement typically comes down to processing requirements and price. For simple pick-and-place requirements such as inserting and removing parts from a mold, a 3-axis robot may be all you need. But a robot is a long-term...

How to Get a 6-Axis Robot for the Price of a 3-Axis
How to Get a 6-Axis Robot for the Price of a 3-Axis

For small and mid-sized manufacturers who are exploring robotics, the decision on 3-axis or 6-axis movement typically comes down to processing requirements and price. For simple pick-and-place requirements such as inserting and removing parts from a mold, a 3-axis robot may be all you need. But a robot is a long-term investment that should meet your requirements today and for years to come. The simple process that you’re considering automating now can easily become more complex over time. You may also find that your initial foray into robotics inspires many new applications for automation, and those may require more sophisticated movement. Fortunately, the decision doesn’t have to be complicated if you can get the advantages of a flexible, long-life 6-axis robot for the price of a 3-axis robot.

A 3-axis robot follows a standard X-Y-Z definition of three-dimensional space. These robots can reach forward and back, from side to side, and up and down. In contrast, a 6-axis robot has an articulated arm that allows for movement that is more similar to that of a human arm. It can rotate, bend, and move in an arc. That maneuverability means these 6-axis robots can grip objects at different angles and can rotate or tilt parts, making them ideal for more sophisticated pick-and-place applications. It typically also makes them more expensive. But every robot arm from Universal Robots offers the cost advantages of a 3-axis robot with the flexibility and maneuverability of a 6-axis robot.

For UR customer Oticon, the world’s second-largest hearing aid manufacturer, that was critical. As hearing aid components became increasingly smaller, Oticon’s older 2- and 3-axis robots were no longer up to the task. For instance, if a small part got stuck in the mold, the robotic arm couldn’t perform the required lateral and vertical movements to tip it out. Oticon installed new, 6-axis UR robot arms, which can easily rotate or tilt parts to lift them quickly out of the mold. The robot’s flexible deployment was also important. Arne Oddershede, group leader of the maintenance unit at Oticon, explains, “Since we produce different batch sizes and components when developing new products, it must be possible to easily reprogram the robot. With a traditional robot, this involves a computer and requires specially-trained staff. But with the UR5, any member of the technical staff can literally grab the robot and show it the motion sequence using waypoints.”

When I started looking, I assumed I was talking hundreds of thousands of dollars per installation. I was surprised to find that we could afford a six-axis robot and a collaborative one at that

Joe McGillivray, Dynamic Group co-owner

Contract manufacturer Dynamic Group found similar advantages. Here, the maneuverable collaborative robot arms from Universal Robots are used in three different applications. Two tend injection-molding machines while the third robot is deployed in a kitting application. First, the UR10 robot picks up the bottom of a custom-made clamshell and then uses a vacuum gripper to pick up two sterile wipes along with some saline solution, placing these into the clamshell. Once items have been placed, the UR10 pushes the full clamshell onto a conveyor and repeats the cycle. These sophisticated motions couldn’t be done with a typical 3-axis robot. Joe McGillivray, Dynamic Group co-owner, originally didn’t think his company could afford collaborative automation. “When I started looking, I assumed I was talking hundreds of thousands of dollars per installation. I was surprised to find that we could afford a six-axis robot and a collaborative one at that.”

McGillivray adds, “I also assumed that I would need a very expensive engineer to help me get these worked out. I’m not an engineer and within an hour of delivery, I had them set up and running basic programs.” The robots have provided improved product consistency and a 400% increase in production capacity, leading McGillivray to estimate the return on investment on the initial system to be less than two months.

If you think you can’t afford the flexibility and maneuverability of a 6-axis robot, now is the time to explore how to get started here with our free ebook.

Universal Robots

We believe that collaborative robotic technology can be used to benefit all aspects of task-based businesses – no matter what their size.

We believe that the latest collaborative robot technology should be available to all businesses. The nominal investment cost is quickly recovered as our robotic arms have an average payback period of just six months.

LinkedIn
Oficina local
  • Universal Robots Mexico SA de CV
  • Bernando Quintana 300
  • 76090 Queretaro, QRO
Contáctenos: 800 877 8005