Tool Drawings

Popis

There are two different mounts for calibration.

  • purchase number: 185500

  • purchase number: 200977

Calibration kit (185500) is with a smaller calibration horse and can be used with the following robots:

All e-Series robots.

 

Calibration kit (number: 200977) is with a larger calibration horse and can be used with the following robots:

UR10e, UR16e and UR Series robots.

 

Calibration Horse (185500)
Only e-Series

The UR3e and the UR10e robot arms are mounted in different positions.

 

Calibration Connector (185500)
Only e-Series

 

 

Calibration Horse (200977)
UR10e, UR16e and UR Series

Calibration Connector (200977)
UR10e, UR16e and UR Series