Functional and Safety Inspection

 
Robot safety functions is highly recommended to be tested monthly to ensure correct function.

Figure 3.1
Numbered instruction per parts of teach pendant.


Emergency stop button on the teach pendant:

  1. Press the emergency stop button of the teach pendant. See figure 3.2.
  2. Observe the robot stops and shuts off power to the joints.
  3. Power on robot again.

 


Figure 3.2
Emergency button of teach pendant.