Thread scheduling
Because the primary purpose of the URScript scripting language is to control the robot, the scheduling policy is largely based upon the realtime demands of this task.
The robot must be controlled a frequency of 500 Hz, or in other words, it must be told what to do every 0.002 second (each 0.002 second period is called a frame). To achieve this, each thread is given a “physical” (or robot) time slice of 0.002 seconds to use, and all threads in a runnable state is then scheduled in a 1 fashion.
Each time a thread is scheduled, it can use a piece of its time slice (by executing instructions that control the robot), or it can execute instructions that do not control the robot, and therefore do not use any “physical” time. If a thread uses up its entire time slice, either by use of “physical” time or by computational heavy instructions (such as an infinite loop that do not control the robot) it is placed in a non-runnable state, and is not allowed to run until the next frame starts. If a thread does not use its time slice within a frame, it is expected to switch to a non-runnable state before the end of 2. The reason for this state switching can be a join instruction or simply because the thread terminates.
It should be noted that even though the sleep instruction does not control the robot, it still uses “physical” time. The same is true for the sync instruction. Inserting sync or sleep will allow time for other threads to be executed and is therefore recommended to use next to computational heavy instructions or inside infinite loops that do not control the robot, otherwise an exception like "Lost communication with Controller" can be raised with a consequent protective stop.