Assembly Screw Connection
| Description |
The assembly is done in reverse of the disassembly. However, a few things must be noted before assembly is begun. Remove old Loctite residue in the screw holes with a roll tap or forming tap (Size 2 M4 the rest M3) for threads before assembling the joint to get the correct torque on the new screws.
Always use new pre-coated screws when possible. If you must assemble with old screws, carefully clean the screws and add Loctite 243 to the screws before assembly. Always replace the black flexible flat ring with a new one to maintain the IP classification. Replace the wear rings if extensive wear or damage is shown |
|
|
|