Wired Connection Setup

Description

In situations where the a 4G connection is either impractical or impossible, you can establish a wired internet connection.

 

To establish a wired connection

  1. Make sure no SIM card is in the router SIM holder.

  2. Use an Ethernet cable to connect to the WAN port of the router.

  3. Connect the router to your network.

When the robot is communicating with the router via your network connection, the PolyScope network screen updates automatically to show the configuration.

To verify the wired connection

  1. Connect a PC to the LAN1 port of the router.

  2. On your PC, open an internet browser and access the router’s administration interface by going to address 192.168.1.1

  3. Login using the name and password on the back of the router.

    If you changed the password, according to previous recommendations, use the new password.

  4. On the Teltonika router dashboard, access the Network->WAN menu, and make sure a WAN connection is active.