Intended Use

Description

The UR Connectivity Kit provides connectivity of UR robots to online services. The UR Connectivity Kit is intended for industrial use, to provide an internet connection to your Universal Robots robot.

The UR Connectivity Kit shall not be used with CB3 robots or PolyScope versions prior to 5.17.

  • Only use UR Connectivity Kit with UR e-Series robots as well as UR20 and UR30 running PolyScope 5.17 or later.

Connecting your Universal Robots robot to the internet requires the integrator and the user to address cybersecurity threats and risks due to physical access to the robot. The mandatory risk assessment of any robot application is required to include a cybersecurity threat assessment, then implementation of the needed cybersecurity measures.

 

Using UR robots or UR products outside of the intended uses can result in injuries, death and/or property damage. Do not use the UR robot or products for any of the below unintended uses and applications:

  • Medical use, i.e. uses relating to disease, injury or disability in humans including the following purposes:

    • Rehabilitation

    • Assessment

    • Compensation or alleviation

    • Diagnostic

    • Treatment

    • Surgical

    • Healthcare

    • Prosthetics and other aids for the physically impaired

    • Any use in proximity to patient/s

  • Handling, lifting, or transporting people

  • Any application requiring compliance with specific hygienic and/or sanitation standards, such as proximity or direct contact with food, beverage, pharmaceutical, and /or cosmetic products.

    • UR joint grease can be released into the air (vapor), or drip.

  • Any use, or any application, deviating from the intended use, specifications, and certifications of UR robots or UR products.

  • Misuse is prohibited as the result could be death, personal injury, and /or property damage

UNIVERSAL ROBOTS EXPRESSLY DISCLAIMS ANY EXPRESS OR IMPLIED WARRANTY OF FITNESS FOR ANY PARTICULAR USE.

  • UR Connectivity Kit is not designed or intended for use in any application requiring compliance with specific hygienic and/or sanitation standards, such as direct contact with food, beverage and/or pharmaceutical products.

  • Any use or application deviating from the intended use, specifications, and certifications is prohibited as the result could be death, personal injury and/or property damage.

  • The UR Connectivity Kit is designed for use in standard industrial environments and is sold “AS-IS”. Universal Robots makes no declaration of conformity, claim of functionality, or fitness for particular purpose to the extent the UR Connectivity Kit is used beyond the prescribed intended use.

  • The user shall ensure that the UR Connectivity Kit is at all times used in full compliance with all applicable regulatory and legal requirements. If the user utilizes the UR Connectivity Kit for applications outside the intended use, the user shall bear sole and exclusive liability.

Failure to use the UR Connectivity Kit in accordance with the intended use can result in unsafe situations.

  • Read and follow the recommendations for intended use provided in this manual.

Failure to use the Teltonika component in accordance with the Teltonika instructions can result in unsafe situations.

  • Read the safety information provided in the Teltonika Wiki accessible by QR code (included with the Teltonika router package).