Software Configuration

Description

The hardware components must be correctly installed before you can set up PolyScope for the Connectivity Kit connection.

 

To establish connection

  1. Make sure the robot is set for Local Control, (otherwise configuration is disabled).

  2. In the top right of the screen, tap the Hamburger menu and select Settings.

  3. In the menu at the left side of the screen, tap System

  4. Select Network.

  5. Then select DHCP to enable networking.

 

When the robot is communicating with the router via your network connection, the PolyScope screen updates automatically to show the configuration.

To disable automatic configuration

Disabling the automatic configuration allows you to set your own configuration.

  1. In the top right of the screen, tap the Hamburger menu and select Settings.

  2. In the menu at the left side of the screen, tap System.

  3. Select Network.

  4. Then select the Static Address option.

Disabling the automatic configuration can lead to network conflicts, which can affect network performance and availability.

You can re-configure the router’s DHCP service which is set to use the entire IP range of the LAN1 subnet. See the Teltonika provided documentation of the router.