Tool Positions
| Description |
Define the Tool Center Point Position at the tip of the screwdriver or nut runner, and the Orientation with the positive Z direction pointing along the tightening axis towards the threaded hole into which the screw will be tightened.
In e-Series the TCP should be copied as a Tool Position in the Safety settings.
|