| Description
|
-
Automatic Screwdriver/Nut Runner: A tool mounted to the robot's tool output flange used for tightening screws or nuts automatically.
-
Base Joint: The first joint of the robot, located at the base.
-
Continuous Fastening: A technique where torque is increased continuously until the target is reached.
-
Elbow Joint: The second joint of the robot, located at the elbow.
-
Fast-Steady Mode: A mode where the robot instantaneously changes into steady mode when torque reaction is detected, allowing higher currents/torques and larger deviations.
-
Force Limits: Restrictions on the forces exerted by the robot at the Tool Center Point (TCP) and elbow joint.
-
Joint Deviations: The difference between the target joint position and the actual joint position, often resulting in protective stop warnings.
-
Joint Torque Maximum Values: The maximum torque values that each joint can withstand.
-
Lever Arm: The perpendicular distance from the axis of rotation to the line of action of a force, used to understand the impact of torque reaction on the robot.
-
Payload: The weight and center of gravity of the load attached to the robot's tool output flange.
-
Protective Stop: A safety mechanism triggered when joint deviations exceed allowed limits.
-
Pulse-Driven Tools: Tools that apply torque in a sequence of increasing pulses, reducing torque reaction compared to continuous fastening.
-
Reaction Devices: Devices mounted on the tool to counteract torque reaction by pushing against the workpiece or fixture.
-
Real-Time Data Exchange: An interface for recording data from the robot, including joint angles, currents, torques, TCP pose, and force.
|
|
|
-
Screwdriving Functionality: An advanced command and installation setup in PolyScope for setting up screwdriving applications, including fast-steady mode.
-
Steady Mode: A state where higher currents/torques are permitted for the robot to maintain its position, and larger deviations are allowed before triggering a protective stop.
-
Target Torque: The desired torque value to be achieved during the screwdriving process.
-
TCP (Tool Center Point): The position at the tip of the screwdriver or nut runner where it contacts the fastener.
-
Torque Arms: Devices used to absorb and transfer reaction force from the robot to an external frame or structure.
-
Torque Reaction: The force transferred to the robot from the tightening process that the robot needs to counteract.
-
Wrist Joint: The final joint of the robot, located at the wrist.
-
Zeroing F/T Sensor: The procedure of calibrating the Force and Torque Sensor without any external forces influencing the readings.
|