Safety Settings
| Description |
The safety system limits the current/torque of each joint according to the force limit, tool positions settings and several other parameters. The tool position should be defined at the tip of the screwdriver or nut runner, where it contacts the fastener. Having the TCP/tool positions configured properly and defining the least restricted tool force limit value that the risk assessment permits, enables the robot arm to handle higher tightening torques from an automatic screwdriver or nut runner.
|