Configurable Safety Functions

Description

Universal Robots robot safety functions, as listed in the table below, are in the robot but are meant to control the robot system i.e. the robot with its attached tool/end effector. The robot safety functions are used to reduce robot system risks determined by the risk assessment. Positions and speeds are relative to the base of the robot.

 

Safety Functions
Safety Function Description

Joint Position Limit

Sets upper and lower limits for the allowed joint positions.

Joint Speed Limit

Sets an upper limit for joint speed.

Safety Planes

Defines planes, in space, that limit robot position. Safety planes limit either the tool/end effector alone or both the tool/end effector and the elbow.

Tool Orientation

Defines allowable orientation limits for the tool.

Speed Limit

Limits maximum robot speed. The speed is limited at the elbow, at the tool/end effector flange, and at the center of the user-defined tool/end effector positions.

Force Limit

Limits maximum force exerted by the robot tool/end effector and elbow in clamping situations. The force is limited at the tool/end effector, elbow flange and center of the user-defined tool/end effector positions.

Momentum Limit

Limits maximum momentum of the robot.

Power Limit

Limits mechanical work performed by the robot.

Stopping Time Limit

Limits maximum time the robot uses for stopping after a protective stop is initiated.

Stopping Distance Limit

Limits maximum distance travelled by the robot after a protective stop is initiated.

 

Risk assessment

When performing the application risk assessment, it is necessary to take into account the motion of the robot after a stop has been initiated. In order to ease this process, the safety functions Stopping Time Limit and Stopping Distance Limit can be used.

These safety functions dynamically reduces the speed of the robot motion such that it can always be stopped within the limits. The joint position limits, the safety planes and the tool/end effector orientation limits take the expected stopping distance travel into account i.e. the robot motion will slow down before the limit is reached.