How to Use This Handbook

Description

Use this handbook to operate robot models using PolyScope X software after powering on the robot.

Before powering on the robot for the first time, please refer to the User Manual:

  • Read the safety information in the robot User Manual that you can find in the box.

  • Make sure that the robot is mounted according to the requirements set in the robot User Manual.

  • Check that the robot arm and the Teach Pendant are connected to the Control Box, and Control Box is connected to the mains power supply.