General safety precautions

Description

Read the general safety precautions before installing the 3PE TP.

For more information on safety, refer to the Safety chapter in the robot User Manual.

 

Installing or maintaining equipment connected to a power source can lead to electric shock.

  • Disconnect the equipment from the power source before installation or maintenance.

 

Incorrect connection of the power source or ground wires can result in equipment damage or personnel injury.

Damage caused by invalid power source connection is not covered by warranty. Before starting the operation:

  • Ensure that the power source wiring is correct.
  • Ensure that the grounding is correct.

 

Failure to verify and validate safeguarding and functionality can result in death or serious injury.

  • Ensure all risk reduction works as intended and achieves the needed risk reduction.

Failure to perform a risk assessment before installation and operation can result in personnel injury or equipment damage.

  • Perform a risk assessment before installation and operation.

  • Read the UR User Manual and UR Service Manual.

 

This product is designed for use as part of the Universal Robots e-Series robot. General safety considerations that are valid for the Universal Robots e-Series robot are also valid for this product.

  • For more information on safety, refer to the Safety section in the Universal Robots e-Series robot User Manual.