Safe Home

Description

Safe Home is a PolyScope X feature that enables users to define a safety-related output that activates when the robot reaches the configured safe home position. The user chooses Home in the dropdown of available smart skill positions, which can be assigned as the reference for the Safe Home position.

 

Access Safe Home

  1. Tap the Application Tab and choose Safety Application. In the left panel, choose Safe Home.

     

     

  2. To configure the robot position, go to Smart Skills Application and choose Home.

  3. Tap the Edit Pose button, and the 3D view of the robot arm appears.

     

 

  1. Jog the robot to the intended position using the Move, Joints, TCP buttons.

  2. Long press the yellow Move Here button until the previewed image is positioned to the new configuration.

  3. Tap Save to finalize the configuration.

     

     

  4. Go back to Safe Home in Safety Application and enter the safety password.

  5. In the activated Smart Skill field, select Home, and the configured robot position appears in the main screen.

  6. Tap Apply and choose Apply and restart. Then tap Confirm Configuration.

     

 

If the Position Smart Skill is selected as the position reference for Safe Home:
  • The message box is displayed on the Position Smart Skill page.

  • The Position Smart Skill configured as Safe Home cannot be renamed, edited, or deleted unless the user deletes or unassigns the Safe Home from the Safety > Safe Home screen.

 

  1. In the Smart Skills screen, the Home position can be duplicated and edited. All the newly created Smart Skills are also available to be configured as Safe Home.

     

     

Safe Home function in outputs

If the Home position is assigned to a position smart skill in Safety, the safety output function dropdown contains Safe Home as a new function assignment.

Choose Safe Home in the Function fields in Outputs of Safety I/O.

 

 

Safe Home can be seen in the table of function assignment on the Confirmation of Applied Safety Configuration overview dialog.

 

 

Safe Home as a program node

The Safe Home program node is located under the Move nodes category within the Command Nodes. This node is used to command the robot to move to its predefined safe home position, as configured in the safety application settings for safe home.

 

Adding the node without a safe home position configured in safety will mark the node as yellow.

 

The Safe Home command node has motion profiles options and other advanced settings when the ellipsis icon is tapped.

 

 

Advanced Settings

Users can create movement profiles in the Advanced Settings using the two tabs and two fields:

  • Motion Profile

  • Speed Type

  • Speed tab

  • Acceleration tab

Motion Profile is a feature enabling users to set predefined motion profiles in move nodes: Joint Move, Linear Move, Circular Arc Move, Process Move, and Direction. Custom Motion Profile enables users to define movement data in move node.

In the Speed Type field, OptiMove is the default option. Choose Classic movement if you want to input speed and acceleration in degrees per second or mm per second. OptiMove settings are specified in percent to simplify the usage and setup.

Users can configure the percentage of preferred speed in the Speed tab, which sets the target travel speed as a percentage of the robot's maximum speed capability.

Users can configure the percentage of preferred acceleration in the Acceleration tab, which sets the target torque limits during acceleration and deceleration as a percentage of the robot's maximum power.