Linear Move

Description

The Linear Move command node supports Motions Profiles as Joint Move, but it creates a movement that is a direct line from point A and point B. It moves the Tool Center Point (TCP) linearly between waypoints. This means that each joint performs a more complicated motion to keep the tool on a straight line path.

 

To access Linear Move command

  1. Go to the main program screen. See Command Nodes.

  2. Tap the Linear Move icon in the Commands toolbox.

    A node with two editable fields, two buttons, and ellipsis icon is inserted into the program tree. These are two editable fields:

    • Motion Profile

    • Name

    These are the three buttons:

    • Edit Point

    • Move Here

  3. Tap the Motion Profile field and select the pertinent from the three choices are available:

    • Custom

    • Linear_fast

    • Linear_slow

 

  1. Tap the Name field, and three tabs appear:

    • Value

    • Variable

    • Expression

  2. Enter the data in the Value, Variable, and Expression tabs, and tap Confirm. See Value-Variable-Expression Tabs.

  3. Tap Edit Point. A new screen appears with the robot arm interface.

  4. Tap More button. The More settings screen appears with four settings:

    • Movement

    • Reference

    • Transform

    • Blend

 

Using the Move Here button

The Move Here button is seen in Linear Move and Joint Move commands. This feature enables you to move to the position of a waypoint directly from the program tree. Pressing the Move Here button opens the Move robot into position dialog. The button is visible when the waypoint has been taught and is only enabled when the robot status is in Normal or Reduced mode.

 

 

  1. Tap the add icon to insert the Linear Move and Joint Move in the command tree.

  2. Tap the Edit Point button of the first move node in the command tree, be it Linear Move or Joint Move nodes.

  3. Jog the robot using the plus-minus button in the X, Y, Z coordinates. Tap Save.

  4. In the second move node in the command tree, tap Move Here. A pop-up screen appears to enable Move robot into position. Long tap Move to Position. Tap Ok.

     

 

Motion Profile labels on Move Nodes

All Move-related command nodes in the program tree display the Motion Profile associated with each node. This feature enables users to see the selected Motion Profile on a Move node. This feature is implemented on the following command nodes:

Move nodes with Custom motion profile will display the values for the speed and acceleration instead of Motion profile.

 

 

Movement setting
  1. Tap the Movement setting on the left side. A Motion Profile field with the following choices appears on the right side. Linear_slow is the default.

    • Custom

    • Linear_fast

    • Linear_slow

  2. If Custom is selected, three more fields appear:

    • Speed Type

    • Speed

    • Acceleration

  3. Choose either OptiMove or Classic when you tap Speed Type.

  4. Tap the Speed field, and the Value, Variable, and Expression tabs pop up.

  5. Enter data in each tab, and tap Confirm. See Value-Variable-Expression Tabs.

  6. Tap the Acceleration field, and the Value, Variable, and Expression tabs pop up.

  7. Enter data in each tab, and tap Confirm. See Value-Variable-Expression Tabs.

  8. When Linear_fast and Linear_slow are selected, the OptiMove speed and acceleration are shown.

 

Reference setting
  1. Tap the Reference setting.

  2. Choose either Frame or TCP field.

  3. In the Frame field, four choices are available:

    • world

    • base

    • flange

    • tcp

  4. In the TCP field, two choices are available:

    • Active_TCP

    • Tool_flange

  5. In the Position column, tap the X, Y, Z tabs and enter your chosen value for the robot, and Confirm.

  6. In the Rotation column, tap the RX, RY, RZ tabs and enter your chosen value for the robot, and Confirm.

 

Transform setting
  1. Tap the Transform setting.

  2. Tap the Pose field and Confirm.

 

Blend setting

  1. Tap the Blend setting.

    A Blend type field appears with two options:

    • Stop at this point

    • Blend

  2. When you choose Stop at this point, no further action is needed but only Confirm.

  3. Tap Blend, and a Radius field is inserted.

  4. The Value, Variable, and Expression tabs pop up when you tap the Radius field.

  5. Enter data in each tab, and tap Confirm. See Value-Variable-Expression Tabs.

  6. To finish, tap Confirm in the More settings screen.