Replacement of Trim Plates Size 2.5, 4, and 5
| Description |
The trim plates on are mounted in a slightly different way depending on the joint size. By applying pressure correctly on the trim plates, it is possible to remove them without any tools. |
Dismounting Trim Plates
|
By pushing the front of the cover you compress the spring so the hooks can be disengaged
|
Mounting Trim Plates
|
By pushing the front of the cover you compress the spring so the hooks can be engaged. The force of the spring will keep the cover in place.
|