Connection Torque Values

 

The clamp connection is present between all joint assemblies.

 
Size Placement Thread Head Size Torque Tolerance
2

UR18 / UR15 / UR8 Long
Wrist 1

Wrist 2

Wrist 3

Tool flange

M4 Hex key 3 2.5 Nm ±10%
2.5

UR20 / UR30

Wrist 1

Wrist 2

Wrist 3

Tool flange

M5 Hex key 4 5.5 Nm ±10%
3

UR18 / UR15 / UR8 Long

Elbow

M5 Hex key 4 4 Nm ±10%
4

UR18 / UR15 / UR8 Long

Shoulder

Base

UR20 / UR30

Elbow

M6 Hex key 5 7.5 Nm ±10%
5

UR20 / UR30

Shoulder

Elbow

M6 Hex key 5 7.5 Nm ±10%

 

Click the torque tool a minimum of three times before use, to get the correct calibrated torque.