항공 제조의 미래 만들기

Ultima Forma

UR10 은 Ultima Forma 가 제로 탄소 항공기 연료 시스템을 위한 파이프를 만드는 데 필수적이며, 공정의 각 단계에서 금속층의 증착을 최대한 제어합니다.

In short

RobotIndus , a certified Universal Robots integrator based in Sarrebourg in the Grand Est region, has developed a test cycle solution for Hansgrohe , a global player in the faucet and sanitary ware sector. Integrated into its production site in Wasselonne in the Grand Est region, the cobotic cell works in close collaboration with operators. Hansgrohe has observed significant productivity gains, as well as an improvement in the working conditions of its employees.

Manual strain meets operational bottleneck

Hansgrohe's initial goal was to improve the ergonomics and efficiency of a machine loading station where operators had to perform several manual operations. The first involved checking the conformity of each assembled shower head by placing it in a water jet testing machine; the three jet types were checked by pressing a button on the edge of the shower head. The operator then manually placed the shower head in front of a blowing machine to extract water and impurities before loading it into a laser marking machine. The final step involved boxing the shower head.

These various repetitive tasks had a negative impact on the health of the operators, who were exposed to musculoskeletal disorders (MSDs). They could experience shoulder and neck pain from handling parts at varying heights. Furthermore, these operations, which, carried out manually, did not represent added value for the company, required a great deal of attention, which was likely to decrease at the end of the day.

After a successful initial cobotic integration on a fairly similar swivel station, Hansgrohe again contacted RobotIndus, a certified integrator (CSI) of Universal Robots, to automate this entire cycle of operations.

RobotIndus

Industry Industrial robotics and automation
Country France
Number of employees 5
Cobot used UR10e

Main value drivers:

  • Simplicity and intuitiveness of the solution
  • Improving workstation ergonomics
  • Increased productivity

Tasks solved by collaborative robots:

  • Loading/unloading machines

Automation challenges solved:

  • Reduction of cycle times
  • Reduction of MSDs among operators
  • Working in hidden time

How they did it

UR10e

Intelligent end-to-end automation with custom engineering

RobotIndus delivered a fully integrated loading and unloading solution for Hansgrohe’s quality control, blowing, and laser marking stations—powered by the Universal Robots UR10e cobot. Equipped with a custom-designed double gripper with suction cups, the cobot handles multiple tasks simultaneously, optimizing cycle time and precision. The system also includes:

  • A circular conveyor with ten green bins and a reject zone
  • A delivery conveyor for final packaging
  • A smart interface with cameras, screens, and illuminated buttons for real-time quality control

This tailored setup transforms a previously manual workflow into a seamless, automated process—designed for speed, accuracy, and ergonomic efficiency.

Building on a successful earlier deployment

Seamless operator experience with minimal training

Despite the complexity of the system, Hansgrohe operators required just half a day of training to master the solution. The intuitive design allows operators to simply place assembled shower heads into green bins. The cobot then:

  • Conducts water jet testing with automatic jet mode switching
  • Uses camera feedback and operator input to identify defects
  • Routes defective units to the reject zone or continues processing through drying, marking, and boxing

The double gripper enables simultaneous loading and unloading, maximizing throughput while keeping the process fluid and operator-friendly.

UR10 모델에서 가장 인상 깊었던 점은 설정의 용이성입니다. 저는 매우 기본적인 코딩 경험으로 이 일을 시작했고, 로봇 공학 경험이나 코봇 (cobots) 은 전혀 경험하지 못했습니다. 그러나 우리는 팔을 상자에서 꺼내 몇 시간 만에 기본 수준으로 올리고 실행했습니다.

Raphael Schwartz, Co-manager of RobotIndus

유니버설 로봇과 연락하세요

수천 개의 기업이 협동 로봇을 활용하여...

  • 생산성 향상
  • 변화하는 제품 수요에 적응
  • 직원 복지 및 유지 개선
  • 노동력 부족 문제 해결
현지 사무소
  • Universal Robots Korea
  • #302, Pankyo Innovalley B
  • 253, Pangyo-ro, Bundang-gu, Seongnam-si, Gyeonggi-do, Korea
문의하기: +82 70 8850 8245