Ultima Forma
RobotIndus , a certified Universal Robots integrator based in Sarrebourg in the Grand Est region, has developed a test cycle solution for Hansgrohe , a global player in the faucet and sanitary ware sector. Integrated into its production site in Wasselonne in the Grand Est region, the cobotic cell works in close collaboration with operators. Hansgrohe has observed significant productivity gains, as well as an improvement in the working conditions of its employees.
Hansgrohe's initial goal was to improve the ergonomics and efficiency of a machine loading station where operators had to perform several manual operations. The first involved checking the conformity of each assembled shower head by placing it in a water jet testing machine; the three jet types were checked by pressing a button on the edge of the shower head. The operator then manually placed the shower head in front of a blowing machine to extract water and impurities before loading it into a laser marking machine. The final step involved boxing the shower head.
These various repetitive tasks had a negative impact on the health of the operators, who were exposed to musculoskeletal disorders (MSDs). They could experience shoulder and neck pain from handling parts at varying heights. Furthermore, these operations, which, carried out manually, did not represent added value for the company, required a great deal of attention, which was likely to decrease at the end of the day.
After a successful initial cobotic integration on a fairly similar swivel station, Hansgrohe again contacted RobotIndus, a certified integrator (CSI) of Universal Robots, to automate this entire cycle of operations.

RobotIndus delivered a fully integrated loading and unloading solution for Hansgrohe’s quality control, blowing, and laser marking stations—powered by the Universal Robots UR10e cobot. Equipped with a custom-designed double gripper with suction cups, the cobot handles multiple tasks simultaneously, optimizing cycle time and precision. The system also includes:
This tailored setup transforms a previously manual workflow into a seamless, automated process—designed for speed, accuracy, and ergonomic efficiency.

Despite the complexity of the system, Hansgrohe operators required just half a day of training to master the solution. The intuitive design allows operators to simply place assembled shower heads into green bins. The cobot then:
The double gripper enables simultaneous loading and unloading, maximizing throughput while keeping the process fluid and operator-friendly.
Raphael Schwartz, Co-manager of RobotIndusUR10 모델에서 가장 인상 깊었던 점은 설정의 용이성입니다. 저는 매우 기본적인 코딩 경험으로 이 일을 시작했고, 로봇 공학 경험이나 코봇 (cobots) 은 전혀 경험하지 못했습니다. 그러나 우리는 팔을 상자에서 꺼내 몇 시간 만에 기본 수준으로 올리고 실행했습니다.
수천 개의 기업이 협동 로봇을 활용하여...