A collaborative robot is a type of industrial robot equipped with a safety function that stops it safely when it comes into contact with an external object such as a person.
The greatest feature of this system is that it can be introduced into the same space as people, without being separated by safety fences, by using robots that comply with the safety requirements set out in safety standards established by the International Organization for Standardization (ISO) and by conducting risk assessments of the system to confirm human safety.
Since Universal Robots first sold collaborative robots in 2008, their adoption has accelerated worldwide, as they are used to automate tasks that traditional industrial robots have given up on automating.
In Japan, the Industrial Safety and Health Regulations (Article 150-4), established in 1983 to prevent industrial accidents, require industrial robots to be enclosed by safety fences and isolated from humans.
The term "industrial robot" was further defined in the Ministry of Labor's Notification No. 51 of the same year as "machines with a drive motor exceeding 80W." This is commonly known as the 80W regulation. Since then, collaboration between industrial robots and humans has been strictly restricted. This regulation reached a turning point in 2013, when a major deregulation was implemented. The Ministry of Health, Labor and Welfare issued Notification No. 1224-2. This now allows industrial robots with an output of 80W or more to be used in collaboration with humans without safety fences, provided they meet the safety requirements set forth in ISO 10218 and ISO/TS 15066 established by the International Organization for Standardization (ISO). Robots that meet these conditions are generally referred to as collaborative robots. The main contents of these standards are as follows:
- (1) Safety-compliant monitoring stops; (2) hand guides; (3) speed and distance monitoring; and (4) power and force limitations due to inherent design or control.
- The safety-related parts of the control systems for these functions must comply with PL=d in a category 3 architecture as specified in ISO 13849-1 or SIL2 as specified in IEC 62061 with a proof test interval of at least 20 years and a hardware fault tolerance of 1.
Universal Robots' collaborative robots have the ability to safely detect and stop force when coming into contact with a person or the outside world, with a reliability of PL=d and Category 3. This satisfies the power and force limitations in condition (4) above, so they can be used in collaborative robot applications.