<link rel="stylesheet" href="styles-JUTMGXX3.css"> Skip to main content

Batch Picking Automation

Increase Throughput by Separating Picking from Consolidation
Universal Robots collaborative robot performing batch picking from conveyor system in an automated warehouse

Scaling Efficiency with Batch Picking Automation

Batch picking improves efficiency by allowing operators to retrieve items for multiple orders in a single trip, reducing travel time and increasing overall productivity. In high-volume environments, however, the gains from batch picking are often limited by downstream constraints. As batch sizes increase, consolidation becomes more complex, congestion rises, and error rates increase—especially when sorting items into individual orders.

MiR AMRs play a central role by transporting batch-picked totes or carts between pick zones and consolidation or packing stations. Unlike manual cart-based systems, MiR AMRs dynamically route based on demand, reducing congestion and maintaining flow even during peak periods.

UR cobots are deployed at the consolidation and packing stage, where repeatability is highest and errors are most costly. This stabilizes the most variable part of the batch picking process and ensures that productivity gains at the picking stage translate into finished orders at the shipping stage.

Advantages of Batch Picking Automation

As with other picking models, orchestration is critical to achieving predictable performance. Systems must coordinate batch release strategies, AMR missions, and station capacity in real time to prevent upstream gains from being lost to downstream congestion. When implemented effectively, batch picking automation becomes a scalable throughput engine capable of handling high order volumes and seasonal peaks without adding proportional labor.

Operational outcomes typically include:

  • Reduced travel time across multiple orders

  • Higher throughput and better utilization of labor

  • Improved accuracy during consolidation and packing

  • Greater resilience during peak demand periods

Case Story DCL Logistics

Robotic Batch Picking Customer Success

At DCL Logistics, UR cobots were deployed in a fulfillment environment to automate picking and packing workflows. The system integrated directly into existing processes and enabled significant improvements in efficiency, labor utilization, and order accuracy—demonstrating how automation at the consolidation and packing stage is critical to scaling high-volume picking operations.

What we’ve seen is up to a 500% increase in productivity by using the robot. The ROI on the robots so far has been three months.

Dave Tu, President. DCL Logistics

Choosing the Right Robotic Picking Automation

Contact our logistics and fulfillment automation team to discover the robotic solution that can meet your picking requirements

Talk to a logistics automation expert

A logistics automation specialist will follow up to review your operations, workflows, and fulfillment challenges. The goal is to understand your setup and identify practical automation opportunities to improve efficiency and scalability—no commitment required.