<link rel="stylesheet" href="app_assets/styles-R77XALWP.css"> Skip to main content

Robotic Packing

Automate packing throughput, consistency, and flow
https://a.storyblok.com/f/169662/2058x2562/1cc7a16562/09_2021_casestory_evcoplastics_-24.jpg

Packing performance is typically constrained by variability at the station and inconsistent flow between picking, packing, and outbound. Robotic packing removes that variability at the point of pack. Universal Robots handle placement and sequencing with repeatable cycle times. While MiR AMRs connect packing to upstream and downstream processes, keeping stations fed and clearing output without manual transport.

The result is a packing operation that runs consistently under load, scales with volume, and stays aligned with upstream picking.

case packing

Where Robotic Packing Fits

Robotic packing is applied where:

  • Packing rates are inconsistent across shifts

  • Product presentation or orientation impacts speed

  • Labor variability affects throughput

  • Flow into or out of packing creates idle time

UR solves the packing task.
MiR stabilizes the flow into and out of the station.

Core Packing Workflows

Why UR + MiR

  • UR stabilizes the pack process (placement, cycle time, repeatability)
  • MiR stabilizes the system (flow, handoffs, coordination)

Together:

  • Eliminate manual transport between steps
  • Maintain consistent throughput across the workflow
  • Allow packing capacity to scale without adding labor
Natura Case Study Universal Robots
Natura logo

Robotic Packing Customer Success

Natura integrated a Universal Robots UR12e collaborative robot into its EKOS production line. Previously, the packing process was carried out manually by two employees. The high volume of packages not only created ergonomic challenges but also required repetitive tasks that added little value to production. Now, the robot handles 70 products per minute.

The introduction UR collaborative robot aligned perfectly with Natura’s mission of innovation and sustainability. The production line handles eight different products, each with its own size and shape. To make this possible, the team implemented a quick-change cobot system that allows three tools to be swapped in just a few minutes. This flexibility lets the collaborative robot adapt easily to different package sizes.

Choosing the Right Robotic Packing Automation

UR20

UR20

Faster heavy payload robot

MiR600

MiR600

Moves pallets up to 600kg

UR16e

UR16e

Heavy-duty compact robot

Talk to a Logistics Automation Expert

A logistics automation specialist will follow up to review your operations, workflows, and fulfillment challenges. The goal is to understand your setup and identify practical automation opportunities to improve efficiency and scalability—no commitment required.