<link rel="stylesheet" href="styles-R77XALWP.css"> Gå til sidens indhold

Payload and working area

Let's define the robots payload and working area.

Robot arm

Robot arm

The robot arm is the center of the work cell. The current 2 product lines consist of 6 arms, ranging from 3 to 30 kg of payload and a working range spanning from 500 mm to around 1.8 meters.

Universal Robots produce articulated 6-degrees of freedom robotic arms. They have built-in safety systems, making them capable of working collaboratively according to ISO 10218-1, if the application and risk assessment allows. Thereby the name, cobots (collaborative robots).

The robot arm consists of 6 rotational joints, each capable of moving ±360 degrees (except for the Wrist Joint on [UR3e/products/ur3-robot), which has limitless rotation).

Robot specifications

Robot specifications

The workspace refers to the total volume or area within which the robot's end-effector can operate or reach. This includes all possible positions and orientations that the end-effector can achieve, taking into account the robot's range of motion and the physical constraints of its joints and links.

It can be complex to determine the precise workspace, as it depends on the end-effector, and highly on the singularities of the robot.

However, a place to start, is to determining the maximum theoretical workspace, which can be seen in the tables below.

Robots

Recommended Reach

Max Working Area

Footprint

UR3e

1000

1146

128

UR5e

1700

1892

151

UR10e

2600

2672

190

UR16e

1800

2002

190

UR20

3500

3571

245

UR30

2600

2695

245

UR3e

UR3e SideviewUR3e Topview

Related links