JL Corp (KSB)
JL Corp (KSB)
JL Corp , a certified Universal Robots integrator based in Lille, Hauts-de-France, has developed an automated water pump wheel balancing solution for KSB , a specialist in valves and pumps. Integrated into its production site in Sequedin, in the Nord department, the cobotic cell is fully secure. Its benefits for the company are numerous, particularly with regard to the quality of finished products, productivity and operator well-being.
The workstation KSB wanted to automate involved balancing water pump impellers, which involves removing material to ensure proper weight distribution across the product. This operation was not only arduous for the operators involved, but also disruptive for the entire production site. On the one hand, it required the lifting of heavy loads, could cause injuries, and was particularly dirty. On the other hand, it generated significant noise pollution, disrupting communication within the teams on site.
In practice, operators had to place the 25 kg wheels on a wheel balancer to determine the amount of material to be removed. They then had to remove them and sand them manually using a grinder—a process that took 30 to 45 minutes. Finally, they placed them back on the wheel balancer to check whether they had removed the correct amount of material.
Performed manually, this operation posed a multitude of problems. Indeed, carrying heavy loads led to musculoskeletal disorders (MSDs), operators could cut themselves while handling the wheels, sanding generated large quantities of dust, and the noise level could exceed 110 dB. As a result, employees dedicated to this position were required to work nights to limit disturbances during the day. In addition, the rendering was often imprecise, requiring the process to be repeated several times before achieving a satisfactory result.
That's why KSB was looking for a solution capable of precisely grinding wheels with reduced noise, while ensuring total operator safety and workplace cleanliness. The company therefore contacted JL Corp, a certified integrator (CSI) of Universal Robots operating in the region.

To address the ergonomic, safety, and precision challenges of manual impeller balancing, JL Corp engineered a fully automated cobotic cell centered around a UR10e collaborative robot, equipped with a fire-resistant protective cover and a Bosch Pro grinder with a cutter attachment. A custom-designed human-machine interface (HMI) tailored for KSB enables intuitive operation and easy parameter updates.
Safety was a top priority: JL Corp conducted a risk analysis with Bureau Veritas, leading to CE certification. The system includes a magnetically secured protective casing to ensure operator safety during operation.
The process now begins with an initial balancing to identify the material to be removed and its location. Operators then use the HMI to input the product reference and removal quantity. Once the cycle starts, the door locks automatically, and the UR10e precisely grinds the impeller based on learned reference points. After grinding, a rebalancing check confirms the accuracy of the operation.
For maintenance, the system includes a dedicated mode that safely repositions the UR10e, allowing quick and secure cutter replacement.

The cobotic solution developed by JL Corp has fully met KSB’s expectations, delivering transformative improvements across safety, productivity, and product quality.
Hugo Marien, Business Manager at JL CorpThe cobotic solution developed by JL Corp has enabled KSB to improve the quality of its water pumps, while ensuring complete operator safety. In addition, it reduces noise pollution and can be started at any time, allowing for more productive work.
Thousands of businesses rely on Collaborative Robots to...