<link rel="stylesheet" href="app_assets/styles-R77XALWP.css"> Skip to main content

Robotic Precision in Powder Coating: Assars’ Automated Touch-Up Solution

In Short

Assars modernized its powder coating operations by implementing an automated touch-up solution combining industrial collaborative robots from Universal Robots with application expertise from Nordbo and intelligent software from Mimic.

The result is a precise, repeatable, and ergonomic process that improves coating quality, reduces manual rework, and supports scalable production.

The Challenge

Powder coating demands consistency, precision, and a high-quality finish. At Assars, manual touch-up work was an essential but challenging part of the process. Operators were responsible for correcting areas where the coating thickness or coverage did not fully meet quality requirements.

While effective, the manual approach created several challenges:

  • Variability in finish quality
  • Physically demanding and repetitive work
  • Time-consuming rework that limited throughput
  • Difficulty scaling without increasing labor

Assars needed a solution that could:

  • Deliver consistent, high-quality touch-ups
  • Reduce manual handling and operator strain
  • Integrate seamlessly into existing coating lines
  • Support future scalability and automation goals

Assars

Industry Surface treatment and powder coating
Country Sweden
Solution Automated powder coating touch-ups
Cobot used UR20
Industrial collaborative robot assisting with spray painting of tall metal panels in a clean, enclosed industrial workspace, while a technician wearing protective gear guides the process.

From manual touch-ups to intelligent automation

To address these challenges, Assars collaborated with Nordbo and Mimic to develop a tailored automation solution.
Industrial collaborative robots from Universal Robots handle the touch-up process with high repeatability, while Nordbo’s application expertise and Mimic’s software ensure precise control and intelligent execution.

The solution allows the robot to apply powder exactly where needed, maintaining consistent quality while eliminating unnecessary over-application.
Because the system is flexible and collaborative, it integrates smoothly into Assars’ existing workflow without major layout changes.

Key value drivers:

  • High precision and repeatability
  • Improved ergonomics and safety
  • Flexible automation
  • Consistent quality

Tasks solved by collaborative robots:

  • Automated powder coating touch-ups

Automation challenges solved:

  • Manual rework and variability
  • Operator fatigue
  • Inconsistent coating thickness
  • Process scalability

With this investment, we have lowered our material consumption by about 25% and thereby reduced our CO2 footprint and simultaneously achieved a better working environment"

Krister Barck, CEO Assars
*With this investment, we have lowered our material consumption by about 25% and thereby reduced our CO2 footprint and simultaneously achieved a better working environment"*

Driving quality through precision and consistency

With automated touch-ups in place, Assars has achieved a more stable and predictable coating process.
The robot delivers uniform application every time, reducing variability and ensuring that finished parts consistently meet quality standards.

This repeatability not only improves product quality but also reduces rework and material waste, supporting a more efficient and sustainable operation.

surface coatingUR20 spray coatingPainted parts drying

One of the key advantages of the solution is its accessibility.
Operators can quickly understand and work with the system, thanks to intuitive programming and collaborative robot design.

Training is hands-on and practical, enabling fast adoption on the shop floor without the need for specialized robotics expertise.
This empowers Assars’ team to focus on quality and process optimization rather than manual correction work.

Looking ahead

What began as a solution for powder coating touch-ups has become a foundation for further automation at Assars.
With a flexible, collaborative setup in place, the company is well positioned to expand automation across additional processes.

By combining industrial collaborative robots from Universal Robots with strong partner expertise from Nordbo and Mimic, Assars is shaping a future-ready powder coating operation built on precision, quality, and people-centered automation.

Get in touch with Universal Robots

Thousands of businesses rely on Collaborative Robots to...

  • Increase productivity
  • Adapt to changing product demand
  • Improve employee well-being and retention
  • Staff through labor shortages