<link rel="stylesheet" href="styles-TODJBD2E.css"> Pular para o conteúdo principal

Machine Communication Interfaces

5 produtos

mostrando

CNC Machine Tending
Robotiq

CNC Machine Tending

Today’s manufacturers want to automate manual tasks with robots, but getting robots up and running is complex, expensive, and can leave you feeling overwhelmed. At Robotiq, we believe robots should simplify your life, not make it more complicated. Working with manufacturers globally (and being one ourselves!), we understand the challenges of maintaining quality, delivering on time, and keeping costs down amidst the labor shortage. Since 2008, Robotiq has pursued its mission of freeing human hands from repetitive tasks by enabling more than 13,000 collaborative robots, or "cobots," worldwide. From SMEs to multinational companies, we're helping manufacturers simplify their processes with easy-to-use automation solutions. Manufacturers want their operations to run smoothly with as little downtime as possible. Automation is often considered, but quickly dropped because of the perception that it is complex and expensive. At Robotiq, we tackle this challenge by making solutions that are actually easy to use. The Machine Tending Solution is the only solution you need to automate your CNC machines. Combined with our worldwide distribution network, you can automate a CNC machine in hours instead of weeks. How can we back that bold statement? The new version of Machine Tending Copilot was developed with the operator in mind. Cobots are simpler to use than industrial robots, but a machine-tending application is still complicated. For this reason, traditional programming can quickly get overwhelming. That’s why our Machine Tending Copilot software guides users through programming from start to finish. With key waypoints and action menus, programming is 75% faster than with traditional methods. Once the key waypoints are created, the user is guided to refine each operation with our action menus—from picking the workpiece to defining pre-programmed cleaning patterns . Since we know that every second counts in the manufacturing process, we’ve created the Smart Move. Using the Machine Tending Copilot algorithm, the robot finds the optimal path from point A to point B without colliding with the environment. This technology can shave up to 15% off your cycle time and shortens setup and downtime, which ultimately gets the machine up and running faster. Earn a quick ROI even with high-mix, low-volume automation; with accelerated program creation, Copilot does the hard work for you. External modules manage communication with the machine interface, so there is no need to open or alter the machine in any way. This approach, which is similar to the way an operator would do the job, makes our solution compatible with almost all machine brands and models. We supply an external control box and pneumatic enclosure to accelerate installation. Custom solutions can be costly and time-consuming to integrate, but the Machine Tending Solution takes less than two hours to deploy and machine your first part—no coding experience required. Elevate your workforce with easy-to-use robot solutions that do the work for you.

Injection Molding Machine Interface (IMMI)
Universal Robots

Injection Molding Machine Interface (IMMI)

The e-Series Injection Molding Machine Interface (IMMI) option provides standardized connectivity between an e-Series robot and injection molding machinery. The IMMI is a separately orderable option for all e-Series robots and supports both EUROMAP 67 and SPI AN-146.

Olympus Colchester Laser Marking Interface
Olympus Technologies

Olympus Colchester Laser Marking Interface

Are your employees fed up manually loading and unloading your laser marking machine? With the Colchester Laser Marking interface, the robot gains the ability to load and start laser marking programs, then wait for the laser marking program to complete, in order to tend the finished part. The Colchester Laser Marking Interface also brings easy-to-use programming to allow a UR to control the Colchester Minilaser XL laser marker. The single programming node and single installation node allow for seamless collaboration between the UR and laser marker.

Robot2CNC - Fanuc FOCAS
VersaBuilt

Robot2CNC - Fanuc FOCAS

The Robot2CNC - Fanuc FOCAS Kit enables Universal Robots to easily execute any machining program stored on a FOCAS enabled Fanuc CNC control while maintaining all CNC safety and execute features.

Robot2CNC Mill Edition
VersaBuilt

Robot2CNC Mill Edition

Robot2CNC - Mill Edition is a controller for CNC machine tending automation. It provides bi-directional CNC communication, CNC cycle start and a pneumatic and IO subsystem to implement virtually any CNC automation application. A URCap plug-in allows a Universal Robot to control all devices through drag and drop teach pendant programming.

Guia de automação

Guia de automação

Encontre a solução de automação e o parceiro certos para o seu negócio
Obtenha apoio personalizado e recomendações de especialistas em 48 horas - totalmente grátis e sem obrigações