<link rel="stylesheet" href="styles-3S7W63VL.css"> Skip to main content

Automatica - World's largest automation fair - e-Series

As CTO and co-founder of Universal Robots, Esben Østergaard, pulled away the black fabric covering the new e-Series cobot at last week’s Automatica fair in Munich, it not only introduced the world to a new collaborative robot line that enables faster development for a wider variety of applications. It also marked the...

Automatica - World's largest automation fair - e-Series
Automatica - World's largest automation fair - e-Series

As CTO and co-founder of Universal Robots, Esben Østergaard, pulled away the black fabric covering the new e-Series cobot at last week’s Automatica fair in Munich, it not only introduced the world to a new collaborative robot line that enables faster development for a wider variety of applications. It also marked a ten year anniversary of the cobot concept being publicly exhibited as a commercially viable automation tool. Back in 2008, as Universal Robots’ modest exhibit opened at Automatica, Universal Robots was the first and only exhibitor to show robots operating outside of safety cages.

“The next day, we were on the front page of the “Messe Zeitung” (the show newspaper). That was really the moment we realized we were on to something,” recounts Esben Østergaard, who has seen his unknown Danish startup grow to become the global market leader, creating a paradigm shift in industrial robotics. His pioneering effort was awarded the Engelberger Robotics award, also known as the Nobel Prize of Robotics, at a ceremony hosted by Robotics Industry Association at Automatica.

Universal Robots at this years Automatica fair 2018

The ‘e’ in the new e-Series stands for Evolution and underpins Universal Robots’ key vision and overall product philosophy of Empowering People and making it Easy for Everyone. With a new built-in, tool-centric Force/Torque sensor the e-Series is ready to take on applications requiring force control right out of the box, such as assembly, sanding, buffing, polishing, and deburring where force-feedback is paramount in order to obtain uniform results. Additionally, the Force/Torque sensor can be used to measure mass and perform related inspection processes or precisely detect contact. A repeatability of 30 micron (0.03mm) in the UR3e and UR5e models and 50 micron (0.05mm) in the UR10e means the new cobots are suitable for very precise finishing, assembly and electronics tasks

The e-Series offers unparalleled convenience; it takes just one hour to unpack the cobot, mount it, and program the first task. A new wrist-joint-tool communication interface reduces production line integration time and the hassle associated with routing cables between the end-effector and control cabinet. As the catalog and capability of UR+ end-effectors have grown so has the need for increased tool power consumption. To address this emerging need the e-Series platform tool power supply now supports up to 2A of peak current. The new cobot line also adds 4 additional digital inputs with an associated interface for use with conveyor tracking

Our CTO and Co-Founder Esben Østergaard received the #Engelberger Award - some call it the "Nobel Prize of Robotics" - a proud moment for all of us at Universal Robots

“End-users with complex applications and diverse or uncertain future needs will benefit from the e-Series platform and our unique Universal Robots+ ecosystem knowing that their investment will be able to grow with them as their needs change,” says President of Universal Robots, Jürgen von Hollen. “We enable innovative customers to rapidly drive the adoption of automation technology into their businesses to maximize their competitive advantage.”

The user interface now also includes programming stopping time and stopping distance for protective stops. This unique feature greatly reduces the complexity and uncertainty involved in performing pre-deployment risk assessments. All 17 safety functions are certified by TÜV Nord and in compliance with the EN ISO 13849-1 and EN ISO 10218-1 machinery safety standards for unobstructed human-robot collaboration.

Universal Robots will start taking orders for the e-Series immediately and begin shipping units to customers from August 1, 2018.

Avatar

Universal Robots

Universal Robots delivers industrial-grade collaborative automation built to perform, scale, and last. Combining lightweight, high-performance hardware with intuitive PolyScope software, certified safety, cybersecurity and open interfaces, Universal Robots enables manufacturers and integrators to deploy automation faster, reduce risk, and evolve toward AI-supported production—across applications, sites, and industries.

Automate with Confidence.