com.ur.urcap.api.contribution
public interface ProgramNodeContribution
Defines an API required for specifying a URCap Program Node within PolyScope.
| Modifier and Type | Method and Description |
|---|---|
void |
closeView()
Called when this node is unselected in the program tree or when navigating to another view.
|
void |
generateScript(ScriptWriter writer)
Defines the script code to be generated by this program node within the
program.
|
String |
getTitle() |
boolean |
isDefined()
Should return true if this program node is complete, and
false otherwise.
|
void |
openView()
Called when this node is selected in the program tree.
|
void openView()
Called when this node is selected in the program tree.
void closeView()
Called when this node is unselected in the program tree or when navigating to another view.
String getTitle()
boolean isDefined()
Should return true if this program node is complete, and false otherwise.
Undefined program nodes will be marked with yellow in the program tree. The user cannot start the program as long as it contains one or more undefined program nodes.
void generateScript(ScriptWriter writer)
Defines the script code to be generated by this program node within the program.
writer - serves to add script commands that define the behaviour of
this program nodeCopyright © 2017. All rights reserved.