Skip to main content

Universal Robots at ATX West 2020

Universal Robots at ATX West 2020
Universal Robots at ATX West 2020

Universal Robots Showcases New Cobot Powered Solutions for Palletizing, Metrology and Machine Tending at ATX West

Attendees at the largest automation technology trade show in the Western U.S. will experience how collaborative robots from industry leader Universal Robots now automate some of the most sought-after tasks in a manufacturing industry facing severe labor shortages.

When manufacturers can't staff tasks on their production lines it severely affects the bottom line resulting in drastic increases in overtime, cycle time and downtime. With the U.S. unemployment rate remaining at 3.5 percent, the lowest in 50 years, 10,000 baby boomers retiring every day and few millennials interested in joining the manufacturing industry, companies are increasingly looking at automation to solve production challenges. At ATX West in Anaheim, CA, Feb 11-13, the pioneer and market leader of collaborative robots, Universal Robots (UR), will show attendees how cobots now power ergonomically unfavorable, repetitive and even technically complex tasks that manufacturers can’t staff.

Fast and Cost-Efficient Palletizing with miniPAL. UR’s ATX booth 4815 is the launch pad for OEM partner Columbia/Okura’s new miniPAL™, a mobile palletizer product powered by the UR10e cobot arm. The flexible miniPAL™ with a footprint of 11’x13’ can palletize at two pallet locations for optimized operation. The latest design showcased at ATX includes two safety mats and two area scanners that detect when people enter the work envelope, allowing the system to meet even higher speeds when not in collaborative mode. The system plugs into 110V AC wall power, can be set up in less than a day, and delivers an average payback between 8-10 months, depending on application and industry.

Columbia/Okura’s miniPAL™ is a plug-and-play (110V), self-contained unit capable of palletizing cases, trays, spot-packs and certain other packages onto any pallet up to 48 inches X 40 inches (GMA & CHEP) dimensions. miniPAL™ comes with easy to use custom pattern building software and features continuous load building capabilities up to 80 inches load heights (package/pattern dependent) onto two pallet locations. Motorized 24vDC infeed conveyor provides reliable pick-up station parameters.

The partnership between Columbia/Okura and UR allows the two companies to provide a safe and economical palletizing solution to clients who are facing labor shortages, many of whom may also be new to factory automation. With the introduction of a collaborative palletizer, employees can be reassigned to work on higher value, less strenuous tasks where their time and skills are better served

Brian Hutton, President of Columbia/Okura LLC.

Parts Inspection in Augmented Reality

Many manufacturers are still using hand tools like calipers, micrometers, or height gages for parts measurement, causing problems with consistency and measurement for complex geometries. 3D scanning provides a more comprehensive inspection report for in-process and final verification for a wide variety of industries. To automate this process, 3D Infotech has developed the UMA Smart Station, a standardized system integrated with Universal Robots collaborative robots. Driven by 3D Infotech’s Streamline software, the UMA station allows for the adding of 3D scanners to the end of UR3e, UR5e and UR10e cobot arms for advanced Scan-to-CAD comparison and inspection capabilities, including GD&T (geometric dimensioning and tolerancing). A recent UMA station customer, Royal Technologies, needed to scan a wide range of parts. “Some operators would miss certain features of the part, resulting in bad parts, now we catch anything that is deviated. To summarize, it has improved speed, quality, and overall performance,” says Trevor Lipsey, launch coordinator at Royal Technologies.

At the show, 3D Infotech will also mount a projector on the cobot arm, projecting inspection results back onto the part through the company’s Spotlight AR++ software, an augmented reality solution that can project colors maps, inspection results, and visual instructions directly on the part. Following the automated 3D scanning and inspection of the part, visitors will be able to visually see the results on the physical object rather than viewing a 2D inspection report. Spotlight AR++ further expands the collaboration between man and machine as the cobot can provide the operator with visual instructions from many points of view.

3D Infotech has introduced the Smart Station integrating UR cobots, 3D scanners, and inspection software to create a configurable automated metrology solution that addresses many challenges faced by manufacturers today. The Smart Station is a robust portable system including a 7th axis rotary table, E-stops, cable management, networking, touch screen monitors, and laptop storage.

At the show, 3D Infotech will also mount a projector on the cobot arm, projecting inspection results back onto the part through the company’s Spotlight AR++ software, an augmented reality solution that can project colors maps, inspection results, and visual instructions directly on the part. Following the automated 3D scanning and inspection of the part, visitors will be able to visually see the results on the physical object rather than viewing a 2D inspection report. Spotlight AR++ further expands the collaboration between man and machine as the cobot can provide the operator with visual instructions from many points of view.

Autonomous Machine Tending in Modular Cell

The UR+ ecosystem of products certified for plug-and-play integration with UR cobots is growing rapidly, now featuring over 200 UR+ products with more than 400 companies in the UR+ developer program. One UR+ partner generating a lot of interest is Vention, with its cloud-based 3D CAD that allows users to easily design, simulate and commission a complete robot cell in as little as three days.

UR+ partner Vention, showcasing its machine tending application which features a UR5e cobot pulling out drawers and picking parts. This application was developed through the company’s MachineBuilder software that allows users to design, simulate and order automation equipment directly through a browser.

Machine tending is one of the most common collaborative robot applications. Despite widespread use, each application requires a somewhat customized robot cell to unlock the full value potential. Vention accelerates the time-to-market with its fully customizable machine tending cells. On display at the UR booth is an example of Vention’s machine tending drawer system that holds parts for a UR5e cobot to pick for machining. Compared to a tray set-up, the drawer system extends the period of autonomous machine tending, as the UR5e simply pulls out a new drawer with more stock once the first drawer is emptied.

Vention will also be showcasing a UR10 cobot at its own ATX booth 5088, featuring the company’s MachineMotion™ controller integrated with the latest URCap (UR+ certified software). This solution allows the cobot to control up to three external drives/actuators in parallel—including ball-screw actuators, belt-driven actuators, rack & pinion actuators and rotational indexers—directly from the Universal Robots pendant. “Universal Robots and Vention are a great product match as we both work towards lowering the automation barrier - reducing upfront investment in time and resources, and accelerating time-to-market. We allow our common customers to get from design to fully functional robot cells in a matter of days,” says Patrick Halde, Vention’s Chief Business Development Officer.

Universal Robots Regional Sales Director for Americas, Stu Shepherd, looks forward to showing the ATX West audience the capabilities and applications now enabled with the new UR+ and OEM partner solutions. “It’s exciting to see our partner network develop new UR cobot powered applications based on market needs. The constant innovation enabled through the UR platform is a great testament to the versatility and relevance of our products.”

Avatar

Universal Robots

Universal Robots delivers industrial-grade collaborative automation built to perform, scale, and last. Combining lightweight, high-performance hardware with intuitive PolyScope software, certified safety, cybersecurity and open interfaces, Universal Robots enables manufacturers and integrators to deploy automation faster, reduce risk, and evolve toward AI-supported production—across applications, sites, and industries.

Automate with Confidence.