Universal Robots on the move - Collaborative Robots

The "Collaborative robot" (cobot) market is booming with more and more businesses looking to improve productivity, efficiency, and drive business growth. With collaborative robots, you can automate most tasks but when you add some wheels and pair a Universal Robots cobot with a mobile robot, the possibilities are endless.

Universal Robots on the move - Collaborative Robots
Universal Robots on the move - Collaborative Robots

The collaborative robot (cobot) market is booming with more and more businesses looking to improve productivity, efficiency and drive business growth. With cobots you can automate most tasks but when you add some wheels and pair a UR cobot with a mobile robot, the possibilities are endless.

Danish company Mobile Industrial Robots (MiR) specializes in automating internal transport and logistics solutions and they currently work with Universal Robots to create effective applications and solutions for business. Their MiR100 is designed to optimize workflows, improve productivity, and reduce costs.

The MiR100 and our UR3 took center stage last year when MiR was presented with the coveted DIRA Automation Award at the tradeshow hi-2015 by the Danish Prime Minister, Lars Løkke Rasmussen. Here the Prime Minister is taking a walk with the MiR100 our UR3.

CEO of MiR, Thomas Visti said there are many benefits available to companies that adopt this type of mobile technology. The combination of the MiR100 and the cobot optimizes production and allows teams and robots to work together.

‘Instead of having a robot arm that’s fixed to one position, manufacturers can now integrate a MiR100 with a Universal Robots’ arm, which can move across the production floor. A great option for pick and place applications.

‘Mobile robots significantly increase productivity because employees aren’t taking time out of their day to move parts around the factory floor. Instead, the parts can be moved by mobile robots which is more efficient. With a combination like this, employees can spend their time focusing on higher-value tasks within the business.

‘We’re seeing this collaboration predominantly being used in the manufacturing industry, however, there’s potential for it to be used across a broad range of industries in the future. Supermarkets for example would benefit greatly from this type of technology to move products around the store and to help restock shelves.

‘The MiR100 and the cobots support each other well, they’re easy to use, set up and they use the same batteries. The flexibility, low cost, and fast return on investment make this type of automation very appealing to business owners’, Visti said.

Taiwan’s largest solar energy automation equipment manufacturer, CASTEC International Corp has developed i-Operator, a robot also integrated with Universal Robots UR5 and UR10 robotic arms.

The MiR100 and our UR3 took centre stage last year when MiR was presented with the coveted DIRA Automation Award at the tradeshow hi-2015 by the Danish Prime Minister, Lars Løkke Rasmussen. Here the Prime Minister is taking a walk with the MiR100 our UR3.
The MiR100 and our UR3 took centre stage last year when MiR was presented with the coveted DIRA Automation Award at the tradeshow hi-2015 by the Danish Prime Minister, Lars Løkke Rasmussen. Here the Prime Minister is taking a walk with the MiR100 our UR3.

The i-Operator is a cobot with computer-integrated manufacturing (CIM) system that’s capable of automated loading and unloading material feeding.

The i-Operator uses a scanned map of particular routes on a factory floor that are coded into the robot by an engineer. The robot can freely move around the factory floor, avoiding obstacles and it has the ability to reroute its path. This prevents interruptions from occurring in the production process and reduces loss in production capacity. This particular technology can work 16 hours a day and uses wireless communication and software control to enhance the accuracy of loading and unloading of materials. Every action performed by the i-Operator is checked by the CIM system to ensure accuracy and productivity.

General Manager of CASTEC, Abel Lo said safety was a key factor in establishing a strong business relationship with Universal Robots.

‘Safety was one of the key factors we took into consideration during the designing of the i-Operator. i-Operator will have to move between employees and perform loading and unloading operations at various workstations in the factory. With the gradual maturing of automated navigation technology, mobile robots are now capable of recognizing and avoiding obstacles and updating the best routes in real-time. Meanwhile, the attached robotic arms must be able to place the materials or products precisely in the correct location. Since loading and unloading operations may be performed at close proximity to other employees around the work station, the safety of the robotic arms is of utmost importance; this is also one of the characteristics offered by the UR robots’, Lo said.

Many semiconductor manufacturers have spent a large amount of time and effort sourcing solutions that can mitigate the labor-intensive material loading and unloading process. The i-Operator is specially designed for semiconductor and LED industries and has been deployed by some Taiwanese manufacturers within their workplaces. These manufacturers have recognized the i-Operator for its effectiveness and influence within the industry.

CASTEC believes the i-Operator can also be deployed in hospitals, restaurants, and hotels in the future and look after tasks like the handling of medical waste. While staff has always handled this type of process, it’s nevertheless a process that poses considerable risk. However with i-Operator, not only would it relieve the busy hospital staff of this mundane task, but it will also reduce occupational hazards and risks.

Discover the endless possibilities of cobots. To find out how you can use this technology in your business click HERE.

Universal Robots

We believe that collaborative robotic technology can be used to benefit all aspects of task-based businesses – no matter what their size.

We believe that the latest collaborative robot technology should be available to all businesses. The nominal investment cost is quickly recovered as our robotic arms have an average payback period of just six months.

LinkedIn
Escritório local
  • Universal Robots España
  • C/ Agricultura, 106
  • 08019 Barcelona
Fale conosco: +34 933 158 076