Replacing the Teach Pendant: Standard TP
This section describes how to remove and replace a Standard Teach Pendant. For information on how to replace a Standard Teach Pendant with a 3PE Teach Pendant, see Replacing the 3PE Teach Pendant.
When the Teach Pendant is replaced, test the E-stop button function.
更换示教盒可能导致系统在启动时报告故障。
- 始终为示教盒类型选择正确的配置。
To remove:
-
关闭控制箱的电源,并从电源上拔下市电电缆。
-
拆除并丢弃用于固定示教盒线缆的两条扎线带。
-
Press in the clips on both sides of the Teach Pendant plug, as illustrated below, and pull down to disconnect from the Teach Pendant port.
-
完全打开/松开控制箱底部的塑料索环,拆除示教盒插头和线缆。
-
轻轻拆除示教盒线缆和示教盒。
To replace:
-
Place the Teach Pendant plug and cable in through the bottom of the Control Box and fully close/tighten the plastic grommet.
-
将示教盒插头推入示教盒端口以连接。
-
使用两条新的扎线带固定示教盒线缆。
-
Connect the main power cable to the power source and power on the Control Box.