UR Connectivity Kit

Description

The UR Connectivity Kit provides internet connection to your Universal Robots robot. It also provides an isolated VLAN (ports LAN2 and LAN3) where up-to two additional units can communicate with each other and with the robot without accessing the internet.

 

Hardware components

The Connectivity Kit hardware components consist the following:

  • A cable gland

  • The Teltonika packaged items:

    • Teltonika RUT951 router

    • Power supply cable to connect the router to a power outlet

    • Ethernet cable to connect the robot to the router

    • Antennas to facilitate 4G & Wifi connection

    • A Teltonika Quick Start Guide to access router safety information

Software requirements

Robots with PolyScope 5.17 as the factory default software will have the full set of cybersecurity features and security settings set by default to restrictive level.

Updating your robot to PolyScope 5.17 introduces new cybersecurity features, but does not change the security settings to restrictive. This requires manual action described in Secure Setup of UR Cobots article.

  • Update the software to PolyScope 5.17.

  • Review the security settings after updating to PolyScope 5.17.

  • Make any necessary adjustments.

See PolyScope in Online Manuals on universal-robots.com/manuals

 

You can also read Secure Setup on www.universal-robots.com/articles

 

As an advanced user, you can reset previously provisioned robots to secure settings by re-imaging the robot SD-card. See How to Replace Flashcards on www.universal-robots.com/articles