Your Product
| Product |
The Base-mounted Range Extender, 40m is an accessory used to extend the cable length between robot and controller. It includes a 40-meter cable (power and communication) and active signal repeaters - one at the robot end and the other at the controller end - for reliable performance over long distances. It is designed for OEM controllers in Welding applications where longer separation between robot and controller is required.
The Base-mounted Range Extender, 40m is compatible with UR3e, UR5e, and UR7e.
The Base-Mounted Range Extender consists of the following components:
This manual describes all of the components. This manual should also be used, if you have purchased any one part as a single component.
|